2009-01-22 07:29 PM
STM32 and WiFi available ?
2011-05-17 03:57 AM
Hi,
I'm searching a OpenSource software stack to run Wifi module with STM32 with SDIO connection up to 48Mhz, I found this Company in US offering a nice solution with a GPL code : and even propose to test it for free for Fix & enhancements. best regards, Asterix.2011-05-17 03:57 AM
(some) Netgear WiFi routers use open source, and the included documentation tells you where to get it...
2011-05-17 03:57 AM
there is a module from RS advertised as WiFi Application Module EDP-AM-WFSD
''... Through hosting a WiFi SD cad, such as Spectec 802.11b card, the module allows communication rates of 11Mbit/s over distances of up to 150m...'' It doesn't say anything about software, but as it is for EDP systems http://rswww.com/edp it must run for example on STR9 (???) Jan2011-05-17 03:57 AM
If an external module will do, look also at
http://www.lantronix.com/device-networking/
and ...http://www.lantronix.com/images/IMG_wiport.jpg
http://www.digi.com/images/products/prd_em_digiconnectwime_sm.jpg
2011-05-17 03:57 AM
(sorry - triplicate post!!)
[ This message was edited by: st7 on 23-01-2009 09:01 ]2011-05-17 03:57 AM
(sorry - duplicate post)
[ This message was edited by: st7 on 23-01-2009 09:00 ]