2009-02-10 08:16 PM
STM32 and system bus
2011-05-17 04:02 AM
Hello all,
I need to interface a CS8900 to STM32, so i need to use the system bus. Can I use the system bus unused pins as GPIOs? Thanks, Lorenzo2011-05-17 04:02 AM
If you'r gonna to interface ISA interface with STM32 through the FSMC, any unused pin either address or data signals can be used as GPIO :-o
2011-05-17 04:02 AM
Quote:
On 11-02-2009 at 00:07, Anonymous wrote: If you'r gonna to interface ISA interface with STM32 through the FSMC, any unused pin either address or data signals can be used as GPIO :-o Thank you! L