cancel
Showing results for 
Search instead for 
Did you mean: 

stm32 adc multi channel

vaibhavsharma63
Associate II
Posted on June 08, 2013 at 12:15

The original post was too long to process during our migration. Please click on the attachment to read the original post.
22 REPLIES 22
vaibhavsharma63
Associate II
Posted on June 14, 2013 at 10:42

hello .do u have sample code in which pressure sensor working with stm32f4discovery

Posted on June 14, 2013 at 13:35

No

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
frankmeyer9
Associate II
Posted on June 14, 2013 at 13:57

I would suggest to seek some local guidance or mentor, as it seems you are not really upt to the task you picked / were assigned to.

There will be no specific example - such a sensor just delivers an analog signal you can measure with the ADC. It is up to you to design and implement the relation between measurement parameter and it's internal representation.