cancel
Showing results for 
Search instead for 
Did you mean: 

Static bits in UID (STM32F4)

danny
Associate

Hey! Does anyone have more info about the UID bits in STM32F4 processors. If I were to use only this processor, which bits could I eliminate from the UID to still have a unique ID for each device and the ID would be the smallest possible in size.

-Thanks

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

The UID consists of X and Y position of the given chip on the wafer, and a number representing the wafer number (this matches ST's manufacturing records). While these numbers concatenated are guaranteed to result in a unique 96-bit number, there's no subset of these bits which result in guaranteed unique number.

JW

Use a hash, or burn your own number in OTP

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..