cancel
Showing results for 
Search instead for 
Did you mean: 

Standard Peripheral Library Documentation

martinkitzberger
Associate II
Posted on April 09, 2015 at 17:51

Hello,

I'm using the standard peripheral library for the STM32F4discovery at the moment because in Cube, there are too many bugs at the moment and so it's currently unuseable for me.

When downloading the standard peripheral library the following documents are included in the extracted folder:

stm32f4xx_dsp_stdperiph_lib_um.html

stm32f4xx_dsp_stdperiph_lib_um.chw

however the problem is, that the html file isn't working and so i can't view all the documention. 

Are there any other documention ressources on the internet about the standard peripherals library cause i really can't find anything usefull, where all the functions are documented.

Example how it could be made:

http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSP432_Driver_Library/latest/exports/driverlib/doc/MSP432P4xx/html/driverlib_html/index.html

Maybe i should switch to this ;)

Thanks for support 

Martin

4 REPLIES 4
Posted on April 09, 2015 at 18:56

In the ST download, or something you extracted/converted elsewhere?

ST provides a Windows .CHM help file.

STM32F4xx_DSP_StdPeriph_Lib_V1.4.0\stm32f4xx_dsp_stdperiph_lib_um.chm

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
martinkitzberger
Associate II
Posted on April 09, 2015 at 23:42

When i download the SP-Library folder from the bottom of this site:

http://www.st.com/web/en/catalog/tools/PF257901

and extract the folder the included file:

stm32f4xx_dsp_stdperiph_lib_um.html

don't works the links are simply missing, or is there any trick how i can open it

that it works?

Posted on April 10, 2015 at 02:01

Are you using Windows? Because neither of the files you name exist in the archive

C:\STMicro\stm32f4_dsp_stdperiph_lib_v1.5.0>dir
Volume in drive C has no label.
Volume Serial Number is D6A0-A0D3
Directory of C:\STMicro\stm32f4_dsp_stdperiph_lib_v1.5.0
04/09/2015 06:39 PM <
DIR
> .
04/09/2015 06:39 PM <
DIR
> ..
03/11/2015 03:17 AM <
DIR
> Libraries
12/31/2014 04:08 AM 17,797 MCD-ST Liberty SW License Agreement V2.pdf
03/11/2015 03:18 AM <
DIR
> Project
03/10/2015 10:34 AM 83,699 Release_Notes.html
03/10/2015 10:43 AM 31,385,441 stm32f4xx_dsp_stdperiph_lib_um.chm
03/11/2015 03:18 AM <
DIR
> Utilities
03/11/2015 03:16 AM <
DIR
> _htmresc
3 File(s) 31,486,937 bytes
6 Dir(s) 437,800,493,056 bytes free

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
martinkitzberger
Associate II
Posted on April 10, 2015 at 10:11

Yes I'm using Windows 8.1.

My directory looks  the same, the .html file is only shown in the Windows 

explorer:

Verzeichnis von C:\Users\marti_000.MARTINACER\Downloads\stm32f4_dsp_stdperiph_l

ib\STM32F4xx_DSP_StdPeriph_Lib

11.03.2015  10:26    <DIR>          .

11.03.2015  10:26    <DIR>          ..

11.03.2015  10:17    <DIR>          Libraries

31.12.2014  11:08            17 797 MCD-ST Liberty SW License Agreement V2.pdf

11.03.2015  10:18    <DIR>          Project

10.03.2015  17:34            83 699 Release_Notes.html

10.03.2015  17:43        31 385 441 stm32f4xx_dsp_stdperiph_lib_um.chm

11.03.2015  10:18    <DIR>          Utilities

11.03.2015  10:16    <DIR>          _htmresc

               3 Datei(en),     31 486 937 Bytes

               6 Verzeichnis(se), 66 253 922 304 Bytes frei

Can I open the .chm file somehow ?