ST32F4: DRAM throughput
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-08-13 4:31 PM
Posted on August 14, 2015 at 01:31
Hi all
I use the STM32429I-EVAL1 board and I did some memory performance measurements (no DMA). The results were a bit strange, as writing to memory is about 50% faster than reading:@180MHz
write mbs/read mbs byte 28.57/14.67 word 136.89/53.05I suspect the memory init code has some errors - for example it doesn't matter what option I use for the burst mode. My init Code looks like this:
sdramHandle.Init.SDBank = FMC_SDRAM_BANK1;
sdramHandle.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4; sdramHandle.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_2; sdramHandle.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE; sdramHandle.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2; sdramHandle.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE; sdramHandle.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_0; sdramHandle.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_9; sdramHandle.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12; sdramHandle.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_32;void BSP_SDRAM_Initialization_sequence(uint32_t RefreshCount){ __IO uint32_t tmpmrd = 0; /* Step 1: Configure a clock configuration enable command */ Command.CommandMode = FMC_SDRAM_CMD_CLK_ENABLE; Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1; Command.AutoRefreshNumber = 1; Command.ModeRegisterDefinition = 0; /* Send the command */ HAL_SDRAM_SendCommand(&sdramHandle, &Command, SDRAM_TIMEOUT); /* Step 2: Insert 100 us minimum delay */ /* Inserted delay is equal to 1 ms due to systick time base unit (ms) */ cyg_thread_delay(1); /* Step 3: Configure a PALL (precharge all) command */ Command.CommandMode = FMC_SDRAM_CMD_PALL; Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1; Command.AutoRefreshNumber = 1; Command.ModeRegisterDefinition = 0; /* Send the command */ HAL_SDRAM_SendCommand(&sdramHandle, &Command, SDRAM_TIMEOUT); /* Step 4: Configure an Auto Refresh command */ Command.CommandMode = FMC_SDRAM_CMD_AUTOREFRESH_MODE; Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1; Command.AutoRefreshNumber = 8; Command.ModeRegisterDefinition = 0; /* Send the command */ HAL_SDRAM_SendCommand(&sdramHandle, &Command, SDRAM_TIMEOUT); /* Step 5: Program the external memory mode register */ tmpmrd = (uint32_t)SDRAM_MODEREG_BURST_LENGTH_4 |\ SDRAM_MODEREG_BURST_TYPE_SEQUENTIAL |\ SDRAM_MODEREG_CAS_LATENCY_2 |\ SDRAM_MODEREG_OPERATING_MODE_STANDARD |\ SDRAM_MODEREG_WRITEBURST_MODE_SINGLE; Command.CommandMode = FMC_SDRAM_CMD_LOAD_MODE; Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1; Command.AutoRefreshNumber = 1; Command.ModeRegisterDefinition = tmpmrd; /* Send the command */ HAL_SDRAM_SendCommand(&sdramHandle, &Command, SDRAM_TIMEOUT); /* Step 6: Set the refresh rate counter */ /* Set the device refresh rate */ HAL_SDRAM_ProgramRefreshRate(&sdramHandle, RefreshCount);}Do you have a clue what could be wrong? BRMichael #dram-throughput
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-08-14 1:29 AM
Posted on August 14, 2015 at 10:29
There could be tens of reasons for that.
How do you get that numbers ? Does the same benchmark returns similar results with the various internal SRAM banks ? Write boost could come from to the effect of the write buffer of the Cortex-M4. Buffering writes gives tremendous bandwidth upgrade particularly with SDRAM. Try to test with write buffer disabled, set bit DISDEFWBUF in ACTLR register from CM4.