cancel
Showing results for 
Search instead for 
Did you mean: 

ST32 2x7 Frame Transmission

julienboulay09
Associate II
Posted on July 09, 2013 at 08:50

Good morning everyone,

I'm currently working on a project with a ST32 and my goal is to be able to give him simple instruction in Modbus TCP/IP thanks to an Ethernet cable. Presently I've been able to code functions in order to get the frame sent to my ST32, check the MAC and IP adresses and the different headers. The only problem is that now, I would like to be able to confirm the good reception of the frame for example when i get a frame in ARP protocole, I'm supposed to answer back with my MAC addresse.

So far I've been reading the reference Manual but the algorythms it gives are pretty blur to me... and so are the different functions proposed in the ETH ST library... If someone had an idea of how I should proceed it would help me very much !

Regards

Julien

3 REPLIES 3
julienboulay09
Associate II
Posted on July 11, 2013 at 08:49

Up ? Anyone ? I really need even the smallest clue...

julienboulay09
Associate II
Posted on July 11, 2013 at 16:18

Solved
sayagyimyo
Associate II
Posted on August 16, 2016 at 05:50

hello mr boulay.julien

I am myo from sg.

I am trying Modbus tcp server on stm32 f207 board.

do u have example code of Modbus tcp ,if  have pls share with me.

my mail is

mailto:sayagyimyo@gmail.com