cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK read protection problem

citroon
Associate
Posted on April 15, 2010 at 21:52

ST-LINK read protection problem

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on May 17, 2011 at 13:47

The only tools I located to do this so far is the Segger J-Link using the JlinkSTM32.EXE program. I typically use U-Link's, and the weren't any good at resolving the ROP setting.

-Clive

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
damh
Associate II
Posted on May 17, 2011 at 13:47

The internal bootloader can do this. Do you have access to the BOOT0 and BOOT1 and USART1 pins?

Set BOOT1=1, BOOT0=0.

Send with 115200,8,E,1 the bytes 0x7F, 0x92, 0x6D.

Then ROP is disabled and flash is erased.

I am using iSystem winIDEA + iC5000. I can set and reset ROP over SWD/Trace.