cancel
Showing results for 
Search instead for 
Did you mean: 

Spirit MP3 Decoder support for hardware float

SORei.1
Associate II

Hello,

     I have a project using the spirit MP3 Decoder. I am in the process of moving this project over to a FreeRTOS based project using the STM32F411. FreeRTOS only supports hardware floating point for this chip and the spirit MP3 decoder is provided as a library only supporting software floating point.

  What is required for me to get a new build of the Spirit MP3 deocder re-compiled supporting hardware floating point?

Can ST provide this re-compiled library?

Thanks

Stuart

0 REPLIES 0