cancel
Showing results for 
Search instead for 
Did you mean: 

SPI2 peripheral on STM32L083RZ

Iwan Attwood
Associate
Posted on November 06, 2017 at 08:30

I have been attempting to use the SPI2 peripheral to drive a flash memory chip using the LL drivers on an STM32L083RZ without success. Microcontroller is the master and flash memory the slave.

The following pins have been configured based on the information in DM00140762

SPI2_SCK  - GPIOB, LL_GPIO_PIN_13, LL_GPIO_AF_0

SPI2_MISO - GPIOC, LL_GPIO_PIN_2,  LL_GPIO_AF_2

SPI2_MOSI - GPIOC, LL_GPIO_PIN_3,  LL_GPIO_AF_2

It is this specific pin configuration I am having problems with, the standard examples for SPI appear to work correctly.

When using the SPI2 peripheral there is apparently no clock generated on Pin 13 of Port B (probed at the MCU pin using an oscilloscope), probing with an oscilloscope does show a sequence of logic level changes on pin 3 of Port C corresponding to the expected data being sent.

Due to time constraints it has been necessary to implement SPI over these pins by bit banging, this is working but loses the ability to use DMA transfers and interrupts. It would be very interested to know if there are limitations in mixing these specific pins with the SPI2 peripheral on the STM32L083RZ

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee
Posted on November 06, 2017 at 16:53

Hello,

Have you checked if you have same condition as described in the related errata sheet.

Otherwise, please try to provide some details in your post and share your configuration or ioc file,  so that it will be easier to understand the issue.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen