cancel
Showing results for 
Search instead for 
Did you mean: 

spi, stm32f7

bks
Associate
Posted on September 07, 2016 at 14:46

Hello, I have a problem with SPI communication for stm32f746-discovery board. I didnt read any value, and when I looked NSS pin is not moving. Only clock is running. SPI is in receive mode only. Function hw_spi_communination() is called on every 1ms.

static void hw_spi_result()
{
for (i = 0; i < 
5
; i++)
{
spi_res += spi_convert_value[i];
}
spi_status->result = spi_res / 5;
}
void HAL_SPI_MspInit(SPI_HandleTypeDef *hspi)
{
GPIO_InitTypeDef gpio_instruct;
//Enable RX clock for SPI
__HAL_RCC_GPIOI_CLK_ENABLE(); // Enable SCK clk
__HAL_RCC_GPIOB_CLK_ENABLE(); // Enable MISO pin
// Enable SPI2 clock
__HAL_RCC_SPI2_CLK_ENABLE();
// Enable DMA clock
__HAL_RCC_DMA1_CLK_ENABLE();
// SPI SCK pin init
gpio_instruct.Pin = GPIO_PIN_1|GPIO_PIN_0;
gpio_instruct.Mode = GPIO_MODE_AF_PP;
gpio_instruct.Pull = GPIO_PULLUP;
gpio_instruct.Speed = GPIO_SPEED_HIGH;
gpio_instruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOI, &gpio_instruct);
// SPI MISO gpio pin init
gpio_instruct.Pin = GPIO_PIN_14;
gpio_instruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOB, &gpio_instruct);
// Config DMA for receive process
dma_handler_rx.Instance = DMA1_Stream3;
dma_handler_rx.Init.Channel = DMA_CHANNEL_0;
dma_handler_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
dma_handler_rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
dma_handler_rx.Init.MemBurst = DMA_MBURST_SINGLE;
dma_handler_rx.Init.PeriphBurst = DMA_PBURST_SINGLE;
dma_handler_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
dma_handler_rx.Init.PeriphInc = DMA_PINC_DISABLE;
dma_handler_rx.Init.MemInc = DMA_MINC_ENABLE;
dma_handler_rx.Init.PeriphDataAlignment = DMA_MDATAALIGN_BYTE;
dma_handler_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
dma_handler_rx.Init.Mode = DMA_CIRCULAR;
dma_handler_rx.Init.Priority = DMA_PRIORITY_MEDIUM;
HAL_DMA_Init(&dma_handler_rx);
// Associate the initialized DMA handle to the the SPI handle
__HAL_LINKDMA(hspi, hdmarx, dma_handler_rx);
// Set DMA1 stream 3 priority.
// When 2 interrupts have same preemption priority, then he one who has higher sub priority will be execute first.
// If both interrupts both have same preemption priority and sub priority, the one comes first will be execute first
HAL_NVIC_SetPriority(DMA1_Stream3_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn);
// Set SPI2 receive priority.
// When 2 interrupts have same preemption priority, then he one who has higher sub priority will be execute first.
// If both interrupts both have same preemption priority and sub priority, the one comes first will be execute first
HAL_NVIC_SetPriority(SPI2_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(SPI2_IRQn);
}
void hw_spi_init()
{
spi_handler.Instance = SPI2;
spi_handler.Init.Mode = SPI_MODE_MASTER;
spi_handler.Init.Direction = SPI_DIRECTION_2LINES_RXONLY; // Receive mode only
spi_handler.Init.DataSize = SPI_DATASIZE_8BIT;
spi_handler.Init.CLKPolarity = SPI_POLARITY_HIGH;
spi_handler.Init.CLKPhase = SPI_PHASE_1EDGE;
spi_handler.Init.NSS = SPI_NSS_SOFT;
spi_handler.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_64; // Baud rate = APB1 / BRprescaler. Max Fsample of MCP3301 is 1,7MHz
spi_handler.Init.FirstBit = SPI_FIRSTBIT_MSB;
spi_handler.Init.TIMode = SPI_TIMODE_DISABLE;
spi_handler.Init.CRCCalculation = SPI_CRCCALCULATION_ENABLE;
spi_handler.Init.CRCPolynomial = 6;
HAL_SPI_Init(&spi_handler);
}
void hw_spi_communination()
{
// Start full duplex communication process.
HAL_SPI_Receive_DMA(&spi_handler, (U8*)spi_convert_value, 5);
}
void DMA1_Stream3_IRQHandler(void)
{
HAL_DMA_IRQHandler(spi_handler.hdmarx);
}
void SPI2_IRQHandler(void)
{
HAL_SPI_IRQHandler(&spi_handler);
}
/*****************************************************************************/
/*****************************************************************************/
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
hw_spi_result();
}

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
bks
Associate
Posted on September 08, 2016 at 09:42

Hello, I found where is the mistake. The schematic of stm32f746-DISCOVERY  board is wrong. PI0 is to output ARD_D5 and PA8 is to output ARD_D10.

Imen.D
ST Employee
Posted on July 20, 2017 at 22:06

Helllo,

I raised this error internally to the appropriate team and it will be corrected in coming release of schematic pack.

The correct assignment in  UM1907 User manual for STM32F746NG.

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen