cancel
Showing results for 
Search instead for 
Did you mean: 

SPI-Slave: unintential continious sending. HELP

beat_blaser
Associate II
Posted on March 01, 2010 at 12:17

SPI-Slave: unintential continious sending. HELP

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Tomas DRESLER
Senior II
Posted on May 17, 2011 at 13:41

Hi Beat,

if master continuously sends clock while nSS line is down, the STM32 peripheral will send last data in the buffer, however reporting underflow. You cannot avoid this as it's a nature of SPI transmission.

Another question is, how to sync the frames. You shall in such case keep the nSS line down during transmission, and rise it up between the frames. It will re-synchronize the slave on the SPI bus.

Another question is, if you use this signaling from the master to STM32.