cancel
Showing results for 
Search instead for 
Did you mean: 

New STM32F2xx zero-wait program execution up to 120MHz

Posted on March 01, 2010 at 13:44

New STM32F2xx zero-wait program execution up to 120MHz

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
supercoolman
Associate II
Posted on May 17, 2011 at 13:41

I haven't seen any standard video processing (x264/NTSC/MPEG) on current Cortex-M3 board yet. And I just bought a STM3210E board few days ago XD

janek2
Associate II
Posted on May 17, 2011 at 13:41

Hi,

 Is there any preliminary preliminary documentation publictly available, or still being a secret?

(As the new devices are already in preliminary sampling stage)

The current consumption is close to that of Energy Micro EFM32 (180uA/MHz)

sampling now.

Jan

BTW, interesting comparison here

http://www.embedded.com/206801769?cid=NL_embedded

 

gahelton1
Associate III
Posted on May 17, 2011 at 13:41

Here is an interesting website. In particular, post #16.

http://bbs.21ic.com/icview-159386-1-1.html

picguy2
Associate II
Posted on May 17, 2011 at 13:41

Do any have EEPROM?  Even 64 bytes would be a BIG help.

I would also like to see some kind of GPIO with DMA.  At least 8 data bits (an option for 16 or possibly 12 data bits would be nice.)  Will need h/w protocol lines.  CPU i/f can assume connected device knows if it is reading or writing.

janek2
Associate II
Posted on May 17, 2011 at 13:41

Hi,

 No EEPROM (you can emulate it), but other things are already on current STM32s. You can do DMA transfer to/from GPIO - see appnote for timer triggered DMA. You can use FSMC to interface to FPGA, LCD, etc.

Jan

Posted on May 17, 2011 at 13:41

Hi,

 Any update on the new device, yet?

Jan