SPI Receive problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-26 9:45 PM
Hi all,
I am trying to read a four bytes register from TDC-GP30 ultrasonic flow converter using HAL_SPI_Receive function. Below is the code that I am using for reading the register contents:
/*******************************************************************************
* Function Name: gp30_read_n_bytes * Parameters: n_bytes = how many bytes should be read * read_opcode = read opcode of the device * read_addr = read address of the device * * Return: n bytes from the specified read address * * Description: Reads n bytes from an address in GP30 * ******************************************************************************/float gp30_read_4_bytes(uint8_t read_opcode, uint8_t read_addr){ uint32_t Result_read = 0x00000000; uint8_t Result_read_buff = 0x00; GP30_SPI_enable(); HAL_SPI_Transmit(&hspi1,&read_opcode,1,100); HAL_SPI_Transmit(&hspi1,&read_addr,1,100); HAL_SPI_Receive(&hspi1,&Result_read_buff,1,100); Result_read |= (Result_read_buff<<24); HAL_SPI_Receive(&hspi1,&Result_read_buff,1,100); Result_read |= (Result_read_buff<<16); HAL_SPI_Receive(&hspi1,&Result_read_buff,1,100); Result_read |= (Result_read_buff<<8); HAL_SPI_Receive(&hspi1,&Result_read_buff,1,100); Result_read |= (Result_read_buff); GP30_SPI_disable(); return Result_read;}The problem is that I cannot receive all four bytes. For example one register contains 0x12345678 and when I read its content I receive 0x12345600 all the time. Its receiving fine for some other values but not for all values.
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-02 10:27 AM
Well my problem become solved simply by changing the input type from float to uint32_t.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-02 3:15 AM
Hi Hashem
I am having problems too, all though I dont have a full understanding of it.
But I would imagine how it works is as follows:
(SPI_HandleTypeDef *hspi, uint8_t *pData, uint16_t Size, uint32_t Timeout)When you use
, the clock pin outputs based on the size of the data (hspi1.Init.DataSize) and the multiplier parameter (which is the third parameter,uint16_t Size
)If your hspi1.Init.DataSize is set to 10bit, and the multiplier is set to 1, then the clock pin will output 10 times.
If the multiplier is set to 2, then the clock pin will output 20 times
However the
parameter (uint8_t *pData) will only transmit on the first 10 bits.
Here I am sending 0xF, 10bit data size, 2 x multiplier
based on the datasheet of the device i am talking to, I cannot use 2 x multiplier. Why? because it will send data during
. And to my understanding, is non blocking mode, which means the application waits for to finish before proceeding with the rest of the program/application.So I would image I would use
with a multiplier of 1, where the clock sends 10 bits.Then I would use
with also a multiplier of 1, causing the clock to sen additional 10bits and also listening on the MISO line.But what actually happens when you use
, it does not send any additional bits on the clock (otherwise i would see it on the oscilloscope) and instead goes to some sort of infinite loop called HardFault_HandlerWhy? this is the third device in a row I have used that has the exact same problem with SPI under the STM32 family.
the varibles I am using:
uint8_t SpiTransmit = 0xF;
uint8_t SpiReceive;calling the HAL functions in main while(1)
HAL_SPI_Transmit(&hspi1, &SpiTransmit, 1, 10);
HAL_SPI_Receive(&hspi1, &SpiReceive, 1, 10);HAL_Delay(100);
initiation code generated from STM32CubeMX 4.19
compiled using Keil uVision v5.23
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-02 7:13 AM
When using spi in bidir mode, the spi clock generation comes from sending out data. Some spi may have rx an tx fifo up to 32 bit chunck capacity. First is to properly write de SPI.DR in 8 or 16 bit mode which will be fifoed. Then the properly configured RXNE will tell when chunk has been received and ready for reading.
There should be some details in the right STM32 Reference Manual.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-02 10:27 AM
Well my problem become solved simply by changing the input type from float to uint32_t.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-03 4:48 AM
I changed
hspi1.Init.DataSize to 8bit, and I am now getting the
/external-link.jspa?url=https%3A%2F%2Fdeveloper.mbed.org%2Fusers%2FEricLew%2Fcode%2FSTM32L4xx_HAL_Driver%2Fdocs%2Ftip%2Fgroup__SPI__Exported__Functions__Group2.html%23gafdf43dbe4e5ef225bed6650b6e8c6313
to send the clock signals, but only 16 in total instead ofThe only problem is, the data that will be sent down the MISO line will be 10 bit.
It seems
/external-link.jspa?url=https%3A%2F%2Fdeveloper.mbed.org%2Fusers%2FEricLew%2Fcode%2FSTM32L4xx_HAL_Driver%2Fdocs%2Ftip%2Fgroup__SPI__Exported__Functions__Group2.html%23gafdf43dbe4e5ef225bed6650b6e8c6313
cannot pass on anything more then 8 bit.So I added another line
/external-link.jspa?url=https%3A%2F%2Fdeveloper.mbed.org%2Fusers%2FEricLew%2Fcode%2FSTM32L4xx_HAL_Driver%2Fdocs%2Ftip%2Fgroup__SPI__Exported__Functions__Group2.html%23gafdf43dbe4e5ef225bed6650b6e8c6313
and got another 8 bit clock signals.Which means if I have two different variables i can then work out the 10bit communicationreceived.
So for anyone one else out there trying to work this out, only use 8bit parameter for
hspi1.Init.DataSize
Thank you KIC8462852 EPIC204278916 for your assistance.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-06 4:05 AM
Just wanted to say the above worked as intended, just have to change
uint8_t SpiReceive;
managed to get values by using unsigned char SpiReceive; instead.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-07-09 2:19 AM
hello hashem
change the type variable