Skip to main content
snafu
Associate II
June 1, 2011
Question

SPI & DMA - DMA irq not called out 2

  • June 1, 2011
  • 1 reply
  • 593 views
Posted on June 01, 2011 at 14:45

Hello,

I encountered problems when trying to send SPI data by means of DMA. It seems that DMA transfer never starts. The sequence of configurations commands is as follow:

1) Enable SPI and DMA clocks

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA, ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

2) Init of DMA

    DMA_DeInit(cfg->txDMAChannel);

    tmpreg |= DMA_PeripheralDataSize_Byte | DMA_MemoryDataSize_Byte | DMA_Mode_Normal | DMA_Priority_VeryHigh | DMA_MemoryInc_Disable | DMA_M2M_Disable| DMA_DIR_PeripheralDST;

    cfg->txDMAChannel->CCR = tmpreg;

3) SPI initialization

   SPI_DeInit(cfg->SPIx);

   cfg->SPIx->CR1 = 0x002F; //BR == 5; MSTR, CPOL, CPHA == 1

   cfg->SPIx->CR2 = 0x03;    //SPI_CR2_TXDMAEN;

4) Enable SPI

   cfg->SPIx->CR1 |= 0x40;

6) Enable DMA irq in NVIC

7) Transaction (transmission) is started as follows

    DMA_Cmd( cfg->txDMAChannel, DISABLE);

    cfg->txDMAChannel->CMAR = (u32)tr->txBuf; //tx buffer ptr

    cfg->txDMAChannel->CPAR = (u32)&cfg->SPIx->DR; //SPI DR reg addr

    cfg->txDMAChannel->CNDTR = (u32)tr->len; //4

    tmp = txDMA->CCR & 0xFF70; /* Clear flags: MINC, TEIE, HTEIE, TCIE, EN */

    tmp |= DMA_MemoryInc_Enable | DMA_IT_TE | DMA_IT_TC;

    cfg->txDMAChannel->CCR = tmp;

   DMA_Cmd(txDMA, ENABLE);

Now I suppose the transaction should get started and after the last send byte, DMA irq should be called out. But nothing like this happens.

When I try to send data without DMA, SPI irq is always called out when TxE is set.

The contents of the relevant registers right after the transaction starts is as follows

DMA_CCR6 == 0x0000309B

DMA_CNDTR == 4

DMA_CPAR ==0x4001300C

DMA_CMAR ==0x200000D4

SPI1_CR1 == 0x6F //BR=5;MSTR, CPOL, CPHA ==1

SPI1_CR2 == 2 // TXDMAEN

SPI1_SR == 2 //TxE

I'll be grateful for any advice or hint.

Thank you
    This topic has been closed for replies.

    1 reply

    snafu
    snafuAuthor
    Associate II
    June 27, 2011
    Posted on June 27, 2011 at 10:06

    I had wrong DMA channel but that was not clear from the snippet. SPI1 uses DMA2 and DMA3 channels.