cancel
Showing results for 
Search instead for 
Did you mean: 

SPI CPOL takes effect only after SPE is set

T YX
Associate
Posted on July 04, 2017 at 05:25

I understand that CPOL takes effect only after SPE is set. But when I talks with AD7606, I need to have CPOL high at idle, and one line only(either BIDIMODE=0 or BIDIMODE=1) for receiving. In this mode, SPE can only be set after NSS is pulled low and that's when the receiving can start. Well now I cannot have SCK high before NSS low and that makes the timing wrong.

Yes I can utilize the full duplex mode and always have SPE set, which makes correct timing. But the transmit line is wasted this way because it's not needed.

Is there a perfect way to talk with this kind of device, which requires SCK high at idle and only a receiving line is used?

Thanks.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User
Posted on July 06, 2017 at 00:22

But the transmit line is wasted this way because it's not needed.

Which STM32? On anything but the F1 you don't need to actually assign any AF to MOSI.

JW

Posted on July 08, 2017 at 11:44

Thanks for replying.

Yes I'm using F101.