cancel
Showing results for 
Search instead for 
Did you mean: 

SPI Beginner-Question (MISO follows CS????)

florianaugustin9
Associate II
Posted on August 16, 2012 at 16:51

Should be okay now, thanks for the attention!

 

 

______________________

 

 

 

 

Dear STM32 experts,

 

 

i'm doing my first SPI bus and i'm coding STM32 for a week now so please don't be too hard :D

 

I'm trying to interface a 

http://www.analog.com/en/mems-sensors/mems-gyroscopes/adxrs450/products/product.html

.

 

So this is my SPI initialization code:

 

---The questions are below the code---

 

void spi3con(void) {

  //Pin Konfiguration: PA15: CS; PC10: SPI3_SCK; PC11: SPI3_MISO; PC12: SPI3_MOSI;

  //SPI1 h�ngt an APB1

  //Clock f�r SPI3 anschalten

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3,ENABLE);

  //GPIO Takt f�r entsprechende Pins anschalten

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA,ENABLE);

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC,ENABLE);

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd  = GPIO_PuPd_UP;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  //Clock-Pin Configuration

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

  GPIO_PinAFConfig(GPIOC,GPIO_PinSource10,GPIO_AF_SPI3);

  //MOSI Configuration

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

  GPIO_PinAFConfig(GPIOC,GPIO_PinSource12,GPIO_AF_SPI3);

  //MISO Configuration

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

  GPIO_PinAFConfig(GPIOC,GPIO_PinSource11,GPIO_AF_SPI3);

  //CS Configuration

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

  //SPI1 Configuration

  //Unselect CHIP --> CS high Pegel

  GPIO_SetBits(GPIOA,GPIO_Pin_15);

  //Full Duplex

  SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;

  //STM32F4 ist Master

  SPI_InitStructure.SPI_Mode = SPI_Mode_Master; 

  //16 bit Modus

  SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b;

  //Clock level zero in idle; clock polarity = 0

  SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;

  //CPHA = 0

  SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;

  //PA15 soll als normaler Pin zu verwenden sein

  SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

  //APB1 = 42 MHz; SCLK max 8,08 MHz; Prescaler --> 8 --> SCLK = 5,25 MHz

  SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8;

  //MSB first (Seite 19 im Datenblatt ADXRS450)

  SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;

  //???? Kein Crc??

  SPI_InitStructure.SPI_CRCPolynomial = 0;

  //SPI3 Einstellungen schreiben

  SPI_Init(SPI3, &SPI_InitStructure);

  //SPI3 einschalten

  SPI_Cmd(SPI3,ENABLE);

}

To test if CS is working i did this in the main function:

 while (1)

  {

   GPIO_SetBits(GPIOA,GPIO_Pin_15);

   delay100ms();

   GPIO_ResetBits(GPIOA,GPIO_Pin_15);

    delay100ms();

  }

Now i see on my logic analyzer that MISO is the same as CS. But CS is like expected. 

 

Is this normal or where is my mistake?

 

There is no shortcircuit in it, it tried it, if i initalize all pins as GPIO everything is okay.

 

And my second question: How can i disable the crc thing for spi? I wrote a zero in it, is that right?

 

 

Thank you for you help!!

 

Best regards,

 

Florian

#stm32f4discovery-spi-cs-miso
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on August 16, 2012 at 17:44

Wouldn't MISO be driven by the SLAVE device? Observe it's behaviour when disconnected from the STM32

One-to-one wiring of MOSI Master, to MOSI Slave, MISO to MISO.

The placement of CS would need to done with attention to where the first and last bits leave the STM32.

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..