SPI and Timer incompatibility?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-06-16 2:28 AM
Posted on June 16, 2014 at 11:28
Hello!
I'm actually trying to use TIM2 interrupt and use SPI in the same time. But when I initialise the SPI peripheral, it doesn't work : there is no timer interrupt any more. You can see above the main function and the useful interrupt functions int main(void) { RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_Init(GPIOD, &GPIO_InitStructure); GPIO_Init(GPIOE, &GPIO_InitStructure); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE, DISABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); GPIO_InitTypeDef gpioinit; gpioinit.GPIO_Mode=GPIO_Mode_IPD; gpioinit.GPIO_Speed=GPIO_Speed_50MHz; gpioinit.GPIO_Pin=GPIO_Pin_12; GPIO_Init(GPIOA, &gpioinit); if (GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_12) != 0) { while (1) { } } /*power on RFM12 module*/ //The SPI peripheral RFM12_poweron(); /*initialize SPI1 peripheral to communicate with RFM12*/ hlperiph_SPI1master_init(); /*initializes RFM12 with correct configuration*/ RFM12_init(); hlperiph_led_init(); hlperiph_EXTI_PA0_init(); uint8_t tx_start[] = ''\r\nStarting main''; //Send a message throught the SPI peripheral RFM12_TxData(tx_start, 15); // SysTick end of count event each 1ms RCC_GetClocksFreq(&RCC_Clocks); SysTick_Config(RCC_Clocks.HCLK_Frequency / 1000); hlperiph_timer2_init(); // RFM12_init(); transmit(); RFM12_poweroff(); /* Infinite loop */ while (1) { } } void TIM2_IRQHandler(void) { if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET) { TIM_ClearITPendingBit(TIM2, TIM_IT_Update); RFM12_init(); uint8_t tx_TIM3[] = ''TIM2''; RFM12_TxData(tx_TIM3, 4); } } Thank you very much, H�lo�se #stm32
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-06-16 5:04 AM
Posted on June 16, 2014 at 14:04
Which STM32? On what board?
Code breaks JTAG/SWD connectivity, so presumably you haven't done any debugging. Code tries to init/send SPI data in an interrupt, this will take a lot of time. Fails to show initialization of TIM, SPI and related GPIOs which would be particularly salient given the posting.
Tips, Buy me a coffee, or three.. PayPal Venmo
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
‎2014-06-17 12:22 AM
Posted on June 17, 2014 at 09:22
STM32F100C4, program through a nucleo board.