cancel
Showing results for 
Search instead for 
Did you mean: 

SPI and DMA transfer

kay
Associate II
Posted on August 22, 2008 at 10:12

SPI and DMA transfer

1 REPLY 1
kay
Associate II
Posted on May 17, 2011 at 12:42

Hi, i have a Problem with a not correct working SPI Transfer.

I use DMA Transfer to load the data register and fetch the rx-data. Furthermore i use hardware nss because i hoped, that the DMA_Channel3->CNDTR

register is reset to initial value when NSS is disabled. But this doesnt seem to be the case? So a lost clock or a clock to much has impact on all further transmissions?! does someone have a solution?