cancel
Showing results for 
Search instead for 
Did you mean: 

Specifications for the F429 DISCO LCD available?

Uwe Bonnes
Principal III
Posted on October 10, 2013 at 15:03

Hello,

are specifications and command descriptions for the LCD Display on the F429 Disco available? It is a SF-TC240T-9370-T type display. Google only brings up information for the SF-TC240T-9229A2-T that doesn't have RGB mode. And even for that display there is no command/register specification.

#sf-tc240t-9370-t #f429-disco #lc
5 REPLIES 5
Uwe Bonnes
Principal III
Posted on October 10, 2013 at 17:18

Thanks!

warcatz
Associate II
Posted on October 10, 2013 at 22:09

Thanx Clive :)

I just get problem with the link to the pdf.

Saef send me this one.

I attach it so if some other get problem with the link it's available here ;)

Cheers.

________________

Attachments :

SF-TC240T-9370A-T_____IC-ILI9341.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzdL&d=%2Fa%2F0X0000000bQg%2FDDT8LcVb9XP7_S_k_.qdBDLWWT5PkKrlQDvpxhw61L4&asPdf=false
gustavo2399
Associate II
Posted on June 15, 2016 at 17:40

Anyone know if the touch is capacitive or resistive?

Thanks!!!

Posted on June 15, 2016 at 22:49

Anyone know if the touch is capacitive or resistive?

Signs point to Resistive

https://media.digikey.com/pdf/Data%20Sheets/ST%20Microelectronics%20PDFS/STMPE811.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..