Something wrong with SDIO
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-14 12:39 AM
there is something wrong with my stm32f427VI while i'm trying to operate sdio.
i am init the sdio interface in pooling mode.
after this ,while i call HAL_SD_WriteBlocks.it's return HAL_ERROR.
and Error code is 16 Transmit FIFO underrun.
but the HAL_SD_ReadBlocks works fine.
can any one help me with this problem,please
this nagged me for many days.
here is my init part:
uint8_t BSP_SD_Init(void)
{ uint8_t SD_state = MSD_OK;uSdHandle.Instance = SDIO;
uSdHandle.Init.ClockEdge = SDIO_CLOCK_EDGE_RISING; uSdHandle.Init.ClockBypass = SDIO_CLOCK_BYPASS_DISABLE; uSdHandle.Init.ClockPowerSave = SDIO_CLOCK_POWER_SAVE_DISABLE; uSdHandle.Init.BusWide = SDIO_BUS_WIDE_1B; uSdHandle.Init.HardwareFlowControl = SDIO_HARDWARE_FLOW_CONTROL_DISABLE; uSdHandle.Init.ClockDiv = SDIO_TRANSFER_CLK_DIV; if (HAL_SD_Init(&uSdHandle) != HAL_OK) SD_state = MSD_ERROR; if (SD_state == MSD_OK) { if (HAL_SD_ConfigWideBusOperation(&uSdHandle, SDIO_BUS_WIDE_4B) == HAL_OK) SD_state = MSD_OK; else SD_state = MSD_ERROR; } return SD_state;}void HAL_SD_MspInit(SD_HandleTypeDef *hsd)
{ if (hsd->Instance == SDIO) {GPIO_InitTypeDef GPIO_Init_Structure;
/* Enable SDIO clock */ __HAL_RCC_SDIO_CLK_ENABLE(); /* Enable GPIOs clock */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); /* Common GPIO configuration */ GPIO_Init_Structure.Mode = GPIO_MODE_AF_PP; GPIO_Init_Structure.Pull = GPIO_PULLUP; GPIO_Init_Structure.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_Init_Structure.Alternate = GPIO_AF12_SDIO; /* GPIOC configuration */ GPIO_Init_Structure.Pin = GPIO_PIN_8 | GPIO_PIN_9 | GPIO_PIN_10 | GPIO_PIN_11 | GPIO_PIN_12; HAL_GPIO_Init(GPIOC, &GPIO_Init_Structure);/* GPIOD configuration */
GPIO_Init_Structure.Pin = GPIO_PIN_2; HAL_GPIO_Init(GPIOD, &GPIO_Init_Structure);}
HAL_StatusTypeDef sd = HAL_SD_WriteBlocks(&uSdHandle, buffer, 1, 1, 100000);//HAL_ERROR
HAL_SD_CardStateTypeDef sta = HAL_SD_GetCardState(&uSdHandle);//HAL_SD_CARD_TRANSFER uint32_t ero = HAL_SD_GetError(&uSdHandle);//ero=16/Transmit FIFO underrunis there anything i missed?or wrong?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-14 7:40 AM
You're supposed to start the card at 400 KHz, not 24 MHz
Personally not a fan of HAL or Polling mode, seem to be a lot of bug reports in current CubeMX release for F4. I'd recommend validating the hardware with the SPL examples.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-14 10:09 AM
I saw that hal libraries start the card with SDIO_INIT_CLK_DIV.
so you recommend me use DMA mode or other SDIO driver?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-14 7:02 PM
I use 4-bit SDIO with DMA, and can typically get 5-8 MBps for writes, and 10-11 MBps for reads, depending on the cards being used. Polling tends to eat bandwidth other tasks could use.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-15 12:23 AM
does the DMA code in cubeMX worked fine,or i need to find some?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-15 7:21 PM
Seems i roll back to 3.7R2 and then problem solved.thanks a lot