Skip to main content
rolfmyhre
Associate II
March 23, 2019
Question

Some hints on using the SWD interface to program devices

  • March 23, 2019
  • 2 replies
  • 721 views

I am soon going crazy! I have used 4 different types of USB -> SWD (Cortex M-10 adapter) programmers like STLINK/V2, Segger J-Link etc. I have made PC boards with several different STM32 MCU types, and what happens is that on some boards the Flash programming goes OK, but in most cases I get some error messages like "DEV NO DEV", "Failed to download application", "Missing device ID code" etc. I have tried to fiddle with general settings like speed and other interface things, but if the card first refuses to be programmed there seems to be no cure - except once when speed adjust worked. CAN ANYONE HELP? Rolf

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    March 23, 2019

    Perhaps start by looking at board design issues.

    Power and reset are primary issues. The JTAG/SWD are usually pretty robust.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    S.Ma
    Principal
    March 23, 2019

    grab a scope, monitor the supply lines if there is an external oscillator check on it, and finally look at the SWD lines, RST AND BOOT0 pin level. I think STLink needs MCU Vdd to checkout its GPIO voltage level too.