2015-08-20 8:14 AM
I want to avoid using a 12MHz external crystal for another IC, so I set the MCO to the PLL, with the HSI feeding the PLL. It works great when I flash the chip, but after a reset, it doesn't work. Everything else in the program functions fine. If I re-flash the STM, it works again until reset.
EDIT: It was a pin config problem. I moved the function that setup the MCO to the beginning of the code without moving the GPIO clock init with it. This thread can be closed. #reset #pll #stm32l151 #mco2015-08-21 4:09 AM
Hi G,
“I moved the function that setup the MCO to the beginning of the code without moving the GPIO clock init with it.�?After reset, all GPIOs are in input mode. So you should reconfigure MCO pin in alternate function mode after reset (SystemInit after PLL activation).-Syrine-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.