cancel
Showing results for 
Search instead for 
Did you mean: 

SOLVED: STM32746G-Discovery STemWin Visual Studio 2015 Build Errors

sisokolov
Associate
Posted on August 23, 2016 at 21:27

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
slimen
Senior
Posted on August 24, 2016 at 11:59

Hi sklv,

There is a Problem when used Visual Studio 2015.

As mentioned in the segger forum from this

http://forum.segger.com/index.php?page=Thread&threadID=2914

, the workaround for this issue is to change the Project Properties as followed:

1. Right-Click on the Project (e.g. SimulationTrial) -> Properties

2 Set Configuration to ''All Configurations''

3. Go to Configuration Properties -> Linker -> Input.

4. Set Ignore All Default Libraries: ''No''

5. Set Ignore Specific Default Libraries: ''LIBC.lib;LIBCMTD.lib''

6. Go to Configuration Properties -> Linker -> Advanced 

7. Set Image Has Safe Exception Handlers:''No (/SAFESEH:NO)'' 

8. Click ''OK''-Button.

Regards

sisokolov
Associate
Posted on August 24, 2016 at 18:57

Hi,

Thanks for your reply. After I followed your instructions, I only had one unresolved symbol:

error LNK2001: unresolved external symbol _sprintf

I added legacy_stdio_definitions.lib to the linker input (https://stackoverflow.com/questions/32418766/c-unresolved-external-symbol-sprintf-and-sscanf-in-visual-studio-2015)

And the simulation compiled and ran.

Thanks again for the input.