2015-08-14 11:09 PM
STM32F103C8
What is the proper setup of a software trigged DMA? Or how do one setup TIM4 so software trigger DMA works? I get a conflict between TIM4 CCR1 match triggered DMA (which works perfectly on it's own)TIM4->DIER |= TIM_DIER_CC1DE; and this software generated DMA trigg
if (buff==1) TIM4->EGR |= TIM_EGR_CC1G; All the software trigger does is gating the TIM4 CCR1 trigger on and off at the speed
of one's and zero's recieved in buff. If i disable TIM4->DIER |= TIM_DIER_CC1DE
and turn TIM4 completely off the software trigger also dies!