2013-08-30 7:07 AM
Good afternoon all,
I am experimenting with the STM32F4Discovery boards and till now I have managed to interface with pin PC0 by connecting a pot and showing the value of its resistance on the LCD touch screen (DM-LCD35RT). Now I wish to make 3 buttons on the touch screen which allows the user to choose between Voltage, Current and Resistance. Each button will show the exact value of the aforementioned variables at that time. Is there an example similar to this project that I can relate to? Thank you all in advance