cancel
Showing results for 
Search instead for 
Did you mean: 

Should an ISR version of an RTOS queue function be called within a callback?

spflanze
Associate II
Posted on September 08, 2015 at 00:11

Within the callback:

HAL_UART_RxCpltCallback()

I need to insert the received character into an RTOS queue. To do this I need to know if I should use the function:

xQueueSendToBack()

or

xQueueSendToBackFromISR()

I know xQueueSendToBackFromISR() should be called within an ISR. What I am not sure about is if it should still be used within a function that is called from an ISR.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0