cancel
Showing results for 
Search instead for 
Did you mean: 

Serial Wire Viewer (SWV) on STM32F100

pcu
Associate II
Posted on December 06, 2012 at 16:52

Hello,

I'm trying to use the serial wire viewer with the STLINK/V2 and the STM32VLdiscovery kit. The embedded debugger is bypassed because it doesn't support SWV.

Debug is OK but there is no signal on SWV. The pin 13 of the debugger is connected to PB3 (TRACESWO). This signal pin is in the Remap function, but I don't know how to reconfigure it (if needed). GPIO_PinRemapConfig() function doesn't define about TRACESWO...

Note: SWV works with my STM3220G-eval but for PB3 there is no remap to do.

Thank you for your help.

Pierre
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
zzdz2
Associate II
Posted on December 06, 2012 at 17:50

I suspect it may be somehow related to the following problem:

 [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/JTAG%20remap%20on%20STM32F103C8T6&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex%5fmx%5fstm32%2fJTAG%20remap%20on%20STM32F103C8T6&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B

If so, it would mean PB3 is really buggy.