cancel
Showing results for 
Search instead for 
Did you mean: 

serial terminal with ymodem and hex string capability

lowpowermcu
Associate II
Posted on August 10, 2011 at 17:15

Hi STM32 users,

I need a serial terminal able to

1. Send file using ymodem file transfer protocol

2. Send hex (not ascii) text format

I was using hyperterminal but it can't send hex format.

I have found hercules but it doesn't support the ymodem protocol.

Is there a tool that supports both ymodem and hex transfer.

MCU Lüfter

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Andrew Neil
Super User
Posted on August 10, 2011 at 17:34

''Send hex (not ascii) text format''

 

What, exactly, do you mean by that?

Do you mean the ability to send the non-printing codes (values 0x00-0x1F) and/or the ''extended'' codes above 0x7F ?
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
lowpowermcu
Associate II
Posted on August 10, 2011 at 17:45

Hi neil,

I want to send the following bitstream:

1122AABBCCDDEEFF

In hercule I did it as in attachement (look at attachment).

________________

Attachments :

hercules_send_hex_string.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0uS&d=%2Fa%2F0X0000000bgg%2F36AFe7PCfv.wlOfDFAc9u07jCHJxQpDor655ng7QhWI&asPdf=false
greg_t
Associate II
Posted on August 10, 2011 at 17:53

Convert HEX to BIN and send it 

trevor23
Associate III
Posted on August 10, 2011 at 17:58

TeraTerm with its script language is quite useful for this kind of thing. It supports y-modem.

John F.
Senior
Posted on August 10, 2011 at 18:14

Also have a look at Docklight.

   

http://www.docklight.de/

lowpowermcu
Associate II
Posted on August 11, 2011 at 11:00

Hi Trevor,

Thank you for your proosal. Now I resolved my problem with teraterm using scripts:

To send the hex string:

Send $11 $22 $33 $44 $55 $66 $77 $C9 $E4 $D4 $54 $B7 $62 $9F $35 $2A

To send the file over ymodem:

ymodemsend srcfile

If there is another tool who can manage the transfer by simple GUI. It will more more helpful.

Thanks again.

MCU Lüfter