2019-07-19 9:27 AM
Hello all,
I am using the h743i eval board and trying to store a large array on the sdram.
The problem I am running into is no matter what address I write to, when I read back a value I receive the last value written. I think this may be an issue with alignment? I am not sure.
My initialization functions are:
static void MX_FMC_Init(void)
{
/* USER CODE BEGIN FMC_Init 0 */
/* USER CODE END FMC_Init 0 */
FMC_SDRAM_TimingTypeDef SdramTiming = {0};
/* USER CODE BEGIN FMC_Init 1 */
/* USER CODE END FMC_Init 1 */
/** Perform the SDRAM1 memory initialization sequence
*/
hsdram1.Instance = FMC_SDRAM_DEVICE;
/* hsdram1.Init */
hsdram1.Init.SDBank = FMC_SDRAM_BANK1;
hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_8;
hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12;
hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_32;
hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3;
hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2;
hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE;
hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_0;
/* SdramTiming */
SdramTiming.LoadToActiveDelay = 16;
SdramTiming.ExitSelfRefreshDelay = 16;
SdramTiming.SelfRefreshTime = 16;
SdramTiming.RowCycleDelay = 16;
SdramTiming.WriteRecoveryTime = 16;
SdramTiming.RPDelay = 16;
SdramTiming.RCDDelay = 16;
if (HAL_SDRAM_Init(&hsdram1, &SdramTiming) != HAL_OK)
{
Error_Handler( );
}
/* USER CODE BEGIN FMC_Init 2 */
/* USER CODE END FMC_Init 2 */
}and
static void SDRAM_Initialization_Sequence(SDRAM_HandleTypeDef *hsdram)
{
FMC_SDRAM_CommandTypeDef Command;
__IO uint32_t tmpmrd =0;
/* Step 1: Configure a clock configuration enable command */
Command.CommandMode = FMC_SDRAM_CMD_CLK_ENABLE;
Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1; //FMC_SDRAM_CMD_TARGET_BANK1
Command.AutoRefreshNumber = 1;
Command.ModeRegisterDefinition = 0;
/* Send the command */
HAL_SDRAM_SendCommand(hsdram, &Command, SDRAM_TIMEOUT);
HAL_Delay(1);
/* Step 3: Configure a PALL (precharge all) command */
Command.CommandMode = FMC_SDRAM_CMD_PALL;
Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1;
Command.AutoRefreshNumber = 1;
Command.ModeRegisterDefinition = 0;
/* Send the command */
HAL_SDRAM_SendCommand(hsdram, &Command, SDRAM_TIMEOUT);
/* Step 4 : Configure a Auto-Refresh command */
Command.CommandMode = FMC_SDRAM_CMD_AUTOREFRESH_MODE;
Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1;
Command.AutoRefreshNumber = 8;
Command.ModeRegisterDefinition = 0;
/* Send the command */
HAL_SDRAM_SendCommand(hsdram, &Command, SDRAM_TIMEOUT);
/* Step 5: Program the external memory mode register */
tmpmrd = (uint32_t)SDRAM_MODEREG_BURST_LENGTH_1 |
SDRAM_MODEREG_BURST_TYPE_SEQUENTIAL |
SDRAM_MODEREG_CAS_LATENCY_3 |
SDRAM_MODEREG_OPERATING_MODE_STANDARD |
SDRAM_MODEREG_WRITEBURST_MODE_SINGLE;
Command.CommandMode = FMC_SDRAM_CMD_LOAD_MODE;
Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1;
Command.AutoRefreshNumber = 1;
Command.ModeRegisterDefinition = tmpmrd;
/* Send the command */
HAL_SDRAM_SendCommand(hsdram, &Command, SDRAM_TIMEOUT);
/* Step 6: Set the refresh rate counter */
/* Set the device refresh rate */
HAL_SDRAM_ProgramRefreshRate(hsdram, REFRESH_COUNT);
}Then my test code is
#define WRITE_READ_ADDR ((uint32_t)0x0800)
#define SDRAM_BANK_ADDR ((uint32_t)0xC0000000)
#define SDRAM_Write32(address, value) (*(__IO uint32_t *) (SDRAM_BANK_ADDR + (address)) = (value))
#define SDRAM_Read32(address) (*(__IO uint32_t *) (SDRAM_BANK_ADDR + (address)))
uint32_t writeval1 = 2045;
uint32_t writeval2 = 7869;
uint32_t readval1 = 0;
uint32_t readval2 = 0;
SDRAM_Write32(WRITE_READ_ADDR, writeval1);
SDRAM_Write32(WRITE_READ_ADDR + 32, writeval2);
/* Read and check */
readval1 = SDRAM_Read32(WRITE_READ_ADDR);
readval2 = SDRAM_Read32(WRITE_READ_ADDR + 32);
sprintf(msgchar, "Val: %lu %lu\n", readval1, readval2);
CDC_Transmit_FS(msgchar, strlen(msgchar));
However readval1 and readval2 are always equal to 7869. By the way, I used CubeMX to generate the FMC init code. Any tips or ideas would be greatly appreciated.
Solved! Go to Solution.
2019-07-25 11:57 AM
Please don't confuse the chip and the board, the latter generally implements a subset of the former
STM32H743I-EVAL I'm aware of has 1x SDRAM and 1x SRAM, where SDRAM != SRAM
2019-07-25 12:34 PM
Clive, I see what you are saying I was trying to drill down from the boards datasheet to what the chip datasheet says about the address mapping.
In any event I found the root cause of the problem: the cubemx tool generated an incorrect HAL_FMC_MspInit() function. Specifically the GPIO_Init pins are wrong, however if I replace these with the GPIO pins specified in the /Examples/FMC/FMC_SDRAM project, the sdram works correctly.
Not sure if its worth letting the CubeMX team know about this but for other people facing the same issue the correct functions in stm32h7xx_hal_msp.c should read:
void HAL_SDRAM_MspInit(SDRAM_HandleTypeDef *hsdram)
{
GPIO_InitTypeDef GPIO_Init_Structure;
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* Enable GPIO clocks */
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOG_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOI_CLK_ENABLE();
/* Enable FMC clock */
__HAL_RCC_FMC_CLK_ENABLE();
/*##-2- Configure peripheral GPIO ##########################################*/
/* Common GPIO configuration */
GPIO_Init_Structure.Mode = GPIO_MODE_AF_PP;
GPIO_Init_Structure.Pull = GPIO_PULLUP;
GPIO_Init_Structure.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_Init_Structure.Alternate = GPIO_AF12_FMC;
/* GPIOD configuration */
GPIO_Init_Structure.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_8| GPIO_PIN_9 | GPIO_PIN_10 |\
GPIO_PIN_14 | GPIO_PIN_15;
HAL_GPIO_Init(GPIOD, &GPIO_Init_Structure);
/* GPIOE configuration */
GPIO_Init_Structure.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_7| GPIO_PIN_8 | GPIO_PIN_9 |\
GPIO_PIN_10 | GPIO_PIN_11 | GPIO_PIN_12 | GPIO_PIN_13 | GPIO_PIN_14 |\
GPIO_PIN_15;
HAL_GPIO_Init(GPIOE, &GPIO_Init_Structure);
/* GPIOF configuration */
GPIO_Init_Structure.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2| GPIO_PIN_3 | GPIO_PIN_4 |\
GPIO_PIN_5 | GPIO_PIN_11 | GPIO_PIN_12 | GPIO_PIN_13 | GPIO_PIN_14 |\
GPIO_PIN_15;
HAL_GPIO_Init(GPIOF, &GPIO_Init_Structure);
/* GPIOG configuration */
GPIO_Init_Structure.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 |\
GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_8 | GPIO_PIN_15;
HAL_GPIO_Init(GPIOG, &GPIO_Init_Structure);
/* GPIOH configuration */
GPIO_Init_Structure.Pin = GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7 | GPIO_PIN_8 | GPIO_PIN_9 |\
GPIO_PIN_10 | GPIO_PIN_11 | GPIO_PIN_12 | GPIO_PIN_13 | GPIO_PIN_14 |\
GPIO_PIN_15;
HAL_GPIO_Init(GPIOH, &GPIO_Init_Structure);
/* GPIOI configuration */
GPIO_Init_Structure.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 | GPIO_PIN_4 |\
GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7 | GPIO_PIN_9 | GPIO_PIN_10;
HAL_GPIO_Init(GPIOI, &GPIO_Init_Structure);
}and
void HAL_SDRAM_MspDeInit(SDRAM_HandleTypeDef *hsdram)
{
/*## Disable peripherals and GPIO Clocks ###################################*/
/* Configure FMC as alternate function */
HAL_GPIO_DeInit(GPIOD, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_3| GPIO_PIN_4 | GPIO_PIN_5 |\
GPIO_PIN_8 | GPIO_PIN_9 | GPIO_PIN_10 | GPIO_PIN_11 | GPIO_PIN_12 |\
GPIO_PIN_13 | GPIO_PIN_14 | GPIO_PIN_15);
HAL_GPIO_DeInit(GPIOE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_3| GPIO_PIN_4 | GPIO_PIN_7 |\
GPIO_PIN_8 | GPIO_PIN_9 | GPIO_PIN_10 | GPIO_PIN_11 | GPIO_PIN_12 |\
GPIO_PIN_13 | GPIO_PIN_14 | GPIO_PIN_15);
HAL_GPIO_DeInit(GPIOF, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2| GPIO_PIN_3 | GPIO_PIN_4 |\
GPIO_PIN_5 | GPIO_PIN_12 | GPIO_PIN_13 | GPIO_PIN_14 | GPIO_PIN_15);
HAL_GPIO_DeInit(GPIOG, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2| GPIO_PIN_3 | GPIO_PIN_4 |\
GPIO_PIN_5 | GPIO_PIN_10);
}
2019-07-25 2:29 PM
I'm not using CubeMX here, things might get fixed/addressed over time, but I have better things to do than QA the product.
Did you select the template/framework for the board?
Hope you were able to make progress on other fronts this week.
2019-07-25 2:35 PM
I am unfortunately using CubeMX but it seems as though the team behind it does not test the code generation properly.
Yes I selected the h743i-eval board when I setup this project.