SDRAM Extended Mode Register Write
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-13 3:26 PM
I am using an STM32F769NI with a MT48H16M32LFB5-6 SDRAM chip, everything works fine. we are looking to set the drive strength to 1/4, 1/2 and full to evaluate the effect on EMC testing. From what I read in the programming manual, it states to perform a dummy read access while BA1=1 and BA=0 in order to select the extended mode register instead of the load mode register and then program the needed value. When I perform the dummy read I receive a hard fault. If anyone can help explain what needs to be done to program the extended mode registers it would be greatly appreciated.
Our configuration is
/* SDRAM device configuration */
sdramHandle.Instance = FMC_SDRAM_DEVICE;
/* Timing configuration for 90Mhz as SDRAM clock frequency (System clock is up to 180Mhz) */
Timing.LoadToActiveDelay = 2;
Timing.ExitSelfRefreshDelay = 8;
Timing.SelfRefreshTime = 3;
Timing.RowCycleDelay = 5;
Timing.WriteRecoveryTime = 2;
Timing.RPDelay = 2;
Timing.RCDDelay = 2;
sdramHandle.Init.SDBank = FMC_SDRAM_BANK1;
sdramHandle.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_9;
sdramHandle.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_11;
sdramHandle.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_32;
sdramHandle.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
sdramHandle.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3;
sdramHandle.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
sdramHandle.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_3;
sdramHandle.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE;
sdramHandle.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_0;
I have tried to read the address and then write the register shown below with no success
BSP_SDRAM_ReadData(0xC1800000, &data, 1);
printf("Val: 0x%08X\r\n", data);
tmpmrd = 0x0040;
Command.CommandMode = FMC_SDRAM_CMD_LOAD_MODE;
Command.CommandTarget = FMC_SDRAM_CMD_TARGET_BANK1;
Command.AutoRefreshNumber = 1;
Command.ModeRegisterDefinition = tmpmrd;
HAL_SDRAM_SendCommand(&sdramHandle, &Command, SDRAM_TIMEOUT);
Thank You,
George Vigelette
Solved! Go to Solution.
- Labels:
-
FMC-FSMC
-
STM32F7 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-13 3:49 PM
Hard Faults because you're beyond the scope of memory
0xC0C00000 would set BA0/BA1=High
0xC0800000 woud set BA0=Low, BA1=High
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
‎2019-06-13 3:49 PM
Hard Faults because you're beyond the scope of memory
0xC0C00000 would set BA0/BA1=High
0xC0800000 woud set BA0=Low, BA1=High
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
‎2019-06-13 3:55 PM
Thank you Clive I will give it a go.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-27 6:22 AM
Worked like a champ thank you !!!