SDIO Multiple Write with STM32F207
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-03-19 8:21 AM
Posted on March 19, 2012 at 16:21
When writing to an SD card in SPI mode, you can do a multiple block write without pre-defining the length (i.e. send CMD25, send some data blocks, finish with a stop command). However, to do a multiple block write using the SDIO functions it seems that the DPSM requires a data length to be set before a write action can occur. Is there any way around this? For example, could I set this to the maximum (512) then cancel/disable the action once the data write is finished?
Thanks in advance. #stm32-sdio
Labels:
- Labels:
-
SDIO-SDMMC
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0