2010-03-08 3:09 PM
SDHC support
2011-05-17 4:42 AM
..Nobody has used a SDHC card here?
2011-05-17 4:42 AM
I've had a 32GB SDHC card running just fine on our hardware but that's using SPI which is of no help to you.
2011-05-17 4:42 AM
Hi Lorenzo,
The SDIO Card driver available with the STM32 Standard Library supports all SD Card types including SD High Capacity. Look at the SD_PowerON function and especially the ''SD_HIGH_CAPACITY'' mask. Regards,2011-05-17 4:42 AM
Thanks Maestro,
I didn't notice it! I'm looking into it, thanks a lot. Lorenzo