2013-06-21 9:47 AM
Is possible to create a file in the SDCARD using only this function?
Consider that the SDCARD was recognized. Mode SPI.SD_CD => PB7SPI1_MOSI => PA7SPI1_SCK => PA5SPI1_MISO => PA6 #spi-sd-card-mmc-stm32f1032013-06-21 11:32 AM
Well it's NOT going to be a FILE
You can write runs of linear data any way you want, it won't be generally readable by anyone else.2013-07-03 5:03 PM
Thanks Clive,
Then I need to useGeneric FAT File System Module
[]2013-07-03 5:11 PM
Yes, you'll need to layer something like FatFs on top of the block IO routines to support a FAT12/FAT16/FAT32 partitioned drive.