cancel
Showing results for 
Search instead for 
Did you mean: 

Scanf-Retarget Problem

shadowrunner92
Associate II
Posted on November 14, 2011 at 11:51

Hello Forum!

While trying to retarget the printf() and scanf() functions, with printf everything worked well. 

However, with scanf occured a weird problem.

First here are the overwrited low-level functions :

size_t __write(int handle, const unsigned char * buffer, size_t size)

{

  size_t nChars = 0;

  if (buffer == 0)

  {

    /*

     * This means that we should flush internal buffers.  Since we

     * don't we just return.  (Remember, ''handle'' == -1 means that all

     * handles should be flushed.)

     */

    return 0;

  }

  for (/* Empty */; size != 0; --size)

  {

    

    while(!(USART1->SR & USART_FLAG_TXE));

      USART1->DR = ((*buffer++) & 0x01FF);

    ++nChars;

  }

  return nChars;

}

size_t __read(int handle, unsigned char * buffer, size_t size)

{

  int nChars = 0;

  for (/* Empty */; size > 0; --size)

  {

    

    while(!(USART1->SR & USART_FLAG_RXNE));

    int c = USART1->DR & 0x01FF;

    if (c < 0)

      break;

    *buffer++ = c;

    ++nChars;

  }

  return nChars;

}

 while (1)

 {

    scanf(''%i \n'',&iNumb);

    printf(''%i\n'',iNumb);

 }

I set a breakpoint into the __read-method() and I noticed something,I think that's the point:

Sending '1', the while-loop becomes true and the integer 'c' equals '1'. (Everythings fine)

The failure is, that the program jumps a second time into the function and get stuck in the while-loop because there's no second character. The result is : sending a second character, the first one is displayed and so on...

For better understanding, here's the Terminal output:

1

2

Echo from STM32: 1

3

Echo from STM32: 2

4

Echo from STM32: 3

5

Echo from STM32: 4

6

Echo from STM32: 5

7

Echo from STM32: 6

8

Echo from STM32: 7

10

Echo from STM32: 8

11

12

Echo from STM32: 1011

The behavior with two-digit numbers is a little different...

Hope you can help me with this one! :)

Thank you in advance!

Chris

1 REPLY 1
clwong88
Associate
Posted on May 04, 2018 at 08:38

Hi Chris,

I wonder if you had solved the problem because I am facing the same problem as your.