cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F413 SPI with DMA safety

sushanth
Associate
Posted on May 04, 2018 at 09:11

Hi,

We are using 2 STM32F413 controllers which are communicationg via the SPI peripheral along with DMA. Ours is a safety critical project we need to add some checks to the DMA as mentioned in the 'UM1840 User manual' - STM32F4 Series safety manual. As we are using the DMA peripheral, we have to take care about the safety aspect of it.

My query is as below

1. As per DMA_SM_1: It speaks about adding the redundanuncy (like CRC or similar). We are already using SPI with the hardware CRC enabled. Do we still need to add another CRC to the data packets?

2. As per DMA_SM_2: Information redundancy including sender or receiver identifier on data packet

transferred via DMA. where and how do we perform this check?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0