cancel
Showing results for 
Search instead for 
Did you mean: 

SAVE MEMORY CONTENTS TO A FILE for STM32F3

love-peace2001
Associate II
Posted on January 29, 2014 at 17:00

Hi all;

I'm working with the discoveryF3  board, i'm using the ST-Link debugger.

I want to save two float arrays into a file when debugging.

My IDE is µVision4.

I found that the command ''save'' can do that  but when i used it, i have wrong values.

Someone has an another technique to this stuff.

Thanks in advance
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on February 04, 2014 at 04:43

I'd just write a PC side app that would run under the Windows Command Line Interface, parse the .HEX, and then print out the floats.

Keil Debugger command line interface

SAVE C:\test3.hex 0x20001234,0x2000123F

SAVE C:\test4.hex 0x20001234,0x20001234+0x1FFF

Windows command line interface

HEX2FLT test3.hex >output

test3.hex

:020000042000DA

:0C123400A4709D3F14AE3642E7875E4474

:00000001FF

output

1.230000

669998

8123474

________________

Attachments :

hex2flt.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzt7&d=%2Fa%2F0X0000000bQl%2FNONTU9ycPO.OXc5BnSLSss3TzXEVUJXCa1IH2.5yGQA&asPdf=false
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..