2014-01-29 6:56 PM
Hi all,
I just started working with STM32F0. I want to try ADC1 in this board but I find some trouble. I want to turn on the LED (PC8 and PC9) by using ADC asbenchmark, so when ADC1 reach 2000 bit or7D0 then LED PC8 and PC9 will tun on.
I've create ADC code and compile it using cocoox, no error. but when I download it to the flash this kode not working. I've try to give input 0-3,2volt to ADC1 (PA1) and the LED is not turn on. this is the code
#include ''stm32f0xx_gpio.h''
#include ''stm32f0xx_rcc.h''
#include ''stm32f0xx_conf.h''
#include ''stm32f0xx_adc.h''
#define ADC_CFGR1_CONT ((uint32_t)0x00002000) /*!< 
Continuous
Conversion */
void pinout_config(void) {
GPIO_InitTypeDef GPIO_InitStruct;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
GPIO_InitStruct.GPIO_Pin
= 
GPIO_Pin_1
; // that's ADC1 (PA1 on STM32)
GPIO_InitStruct.GPIO_Mode
= 
GPIO_Mode_AN
;
GPIO_InitStruct.GPIO_PuPd
= 
GPIO_PuPd_NOPULL
;
GPIO_Init(GPIOA, &GPIO_InitStruct);
ADC_Cmd (ADC1,ENABLE); //enable ADC1
}
void led_config(void){
GPIO_InitTypeDef GPIO_InitStruct;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);
/*Configure GPIO pin */
GPIO_InitStruct.GPIO_Pin
= 
GPIO_Pin_8
|GPIO_Pin_9;
GPIO_InitStruct.GPIO_Mode
= 
GPIO_Mode_OUT
;
GPIO_InitStruct.GPIO_OType
= 
GPIO_OType_PP
;
GPIO_InitStruct.GPIO_PuPd
= 
GPIO_PuPd_NOPULL
;
GPIO_InitStruct.GPIO_Speed
= 
GPIO_Speed_2MHz
;
GPIO_Init(GPIOC, &GPIO_InitStruct);
}
int main(void)
{
pinout_config();
led_config();
while(1)
{
void LED_set (void)
{
if(ADC1>2000)
{
(GPIOC->BSRR = GPIO_Pin_8);
(GPIOC->BSRR = GPIO_Pin_9);
}
else {
(GPIOC->BRR = GPIO_Pin_8);
(GPIOC->BRR = GPIO_Pin_9);
}
}
}
}
can someone tell me what is wrong with the code?
thank you for your help
2014-01-29 8:17 PM
Lack of compilation errors means no syntax issues, it doesn't mean the code is valid. Your example lacks configuration of the ADC, and association of the pin with the channels to be sampled.
/* ADC1 STM32F0-Discovery sourcer32@gmail.com */
#include ''stm32f0xx.h''
#include ''stm32f0_discovery.h''
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOC, ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; // PA.1 ADC IN1
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOC, &GPIO_InitStructure);
}
void ADC1_Configuration(void)
{
ADC_InitTypeDef ADC_InitStructure;
/* ADC1 DeInit */
ADC_DeInit(ADC1);
/* ADC1 Periph clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
/* Initialize ADC structure */
ADC_StructInit(&ADC_InitStructure);
/* Configure the ADC1 in continous mode withe a resolutuion equal to 12 bits */
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward;
ADC_Init(ADC1, &ADC_InitStructure);
/* Convert the ADC1 input with 5 Cycles as sampling time */
ADC_ChannelConfig(ADC1, 1, ADC_SampleTime_55_5Cycles); // PA.1 - IN1
/* ADC Calibration */
ADC_GetCalibrationFactor(ADC1);
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);
/* Wait the ADCEN falg */
while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_ADEN));
/* ADC1 regular Software Start Conv */
ADC_StartOfConversion(ADC1);
}
int main(void)
{
GPIO_Configuration();
ADC1_Configuration();
while(1)
{
uint16_t ADC1ConvertedValue;
/* Test EOC flag */
while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);
/* Get ADC1 converted data */
ADC1ConvertedValue = ADC_GetConversionValue(ADC1);
if (ADC1ConvertedValue > 2000)
{
GPIOC->BSRR = GPIO_Pin_8;
GPIOC->BSRR = GPIO_Pin_9;
}
else
{
GPIOC->BRR = GPIO_Pin_8;
GPIOC->BRR = GPIO_Pin_9;
}
}
}2014-01-29 10:10 PM
thanks for your respon clive.
I've try debug your code to my board but it doesn't work and in my compiler apear a message (No source available for '''') this link to my compile screen capture2014-01-29 11:29 PM
in console tab this message appear
Reading symbols from C:\CooCox\CoIDE\workspace\ADC Rev1.2\ADC Rev1.2\Debug\bin\ADC Rev1.2.elf...done.
file ''C:/CooCox/CoIDE/workspace/ADC Rev1.2/ADC Rev1.2/Debug/bin/ADC Rev1.2.elf''
file ''C:/CooCox/CoIDE/workspace/ADC Rev1.2/ADC Rev1.2/Debug/bin/ADC Rev1.2.elf'' set tdesc filename C:/CooCox/CoIDE/bin/target_desc/arm-with-m.xml target remote 127.0.0.1:2009 Reset_Handler () at C:\CooCox\CoIDE\workspace\ADC Rev1.2\cmsis_boot\startup\startup_stm32f0xx.s:74 74 movs r1, #0tbreak main
Temporary breakpoint 1 at 0x800049e: file C:\CooCox\CoIDE\workspace\ADC Rev1.2\main.c, line 66.continue
Temporary breakpoint 1, main () at C:\CooCox\CoIDE\workspace\ADC Rev1.2\main.c:66 66 GPIO_Configuration();kill
I have no idea about it. what should I do?2014-01-30 11:20 AM
I have no idea about it. what should I do?
Use a different tool chain? I don't use CooCox, suggest you download an evaluation of Keil uv 4.7x2014-02-03 7:13 PM
I found the problem.I have not entered this code
ADC_ChannelConfig(ADC1,ADC_Channel_1,ADC_SampleTime_1_5Cycles);