cancel
Showing results for 
Search instead for 
Did you mean: 

Sampling Freqeuncy for the ADC STM32F4

mahmoud
Associate
Posted on August 28, 2013 at 12:47

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on August 28, 2013 at 14:15

I'd use a timer to pace samples.

Your USART output speed is likely to be bandwidth limiting.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mahmoud
Associate
Posted on August 28, 2013 at 14:46

Dear Clive,

Thank you for your fast response ! :)

But is there a method to get the sampling frequency without using a timer routine ?

i will keep it as it is ... but i need to know the sampling rate since i need to write some codes using MATLAB .... 

cheers

Posted on August 28, 2013 at 16:17

Give the way your code is constructed, I guess you'd want to time stamp the EOC.

Personally, I wouldn't be using SCAN mode as you only have ONE channel. If you want to control the sample rate via the ADC, then you'd want to program the cycles, and use it in CONTINUOUS mode.

Using software delay loops, and manually firing the ADC are not ways to get consistent sample periodicity.

I'd trigger it with a timer, and have a hard/known time line.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..