Skip to main content
imichalev
Visitor II
January 8, 2011
Question

RTC_SetCounter() function ;

  • January 8, 2011
  • 0 replies
  • 481 views
Posted on January 08, 2011 at 23:15

I've have problem with  

RTC_SetCounter()  function .

When I use 

RTC_SetCounter() mine program stopped in the next function  

RTC_WaitForLastTask() ;

I tried this metod  :

        

PWR_BackupAccessCmd(ENABLE);

     /* Wait until last write operation on RTC registers has finished */

     RTC_WaitForLastTask();

     /* Set initial value */

     RTC_SetCounter(0x0); 

     /* Wait until last write operation on RTC registers has finished */

     RTC_WaitForLastTask();

     PWR_BackupAccessCmd(DISABLE);

,but it doesn't solve the problem :( .What  can I do ? 

I use stm32 discovery board with external power for backup domain Vbat=3v , and removed SB1 from factory board.

I'am sorry but there was  my fault .I forgot to set clk for backup domain .

 RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR |RCC_APB1Periph_BKP ,ENABLE); 

I do this when configuration bckdomain for the first time , and next time when start up board I was missing to do that.

#stm32
    This topic has been closed for replies.