cancel
Showing results for 
Search instead for 
Did you mean: 

RTC running fast on STM32L433

Scott Dev
Senior

Hi

I have setup the RTC on the STM32L433 and the clock is running about 5 second fast in 24 hours. I am using a 32.768KHz crystal, which is directly next to the processor . I have set the

RTC->PREDIV_A to 0x 7f, and RTC->PREDIV_A to 0x ff, and selected the LSE clock, cant think what it can be, anyone help?

Thanks

Scott

13 REPLIES 13

Double check the measured frequency. Should be able to benchmark via a connected TIM, or if available on an MCO pin.

Check loading, check trim settings.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Principal III

5 second in a day is about 60 ppm. Crystal tolerance is oftne 50 ppm plus some load capacitance mismatch and your number can be explained.

You can use TIM16

Example here for measuring LSI here, but can select LSE

STM32Cube_FW_L4_V1.13.0\Projects\NUCLEO-L432KC\Examples\RTC\RTC_LSI\Src\main.c

The math here is broken, destroys accuracy

  /* Frequency computation */

  uwLsiFreq = (uint32_t) SystemCoreClock / uwPeriodValue;

  uwLsiFreq *= 8;

Use

  uwLsiFreq = (SystemCoreClock * 8) / uwPeriodValue;

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Peter Mather
Associate III

Use HAL_RTCEx_SetSmoothCalib to tune the frequency. Here is my clock set up. Note Prediv setting are different to allow sub second reading

The calibration value (Option.RTC_calibrate in my code) can be between -511 and + 512. n specifies the number of extra clock pulses to be "created" or "removed" every 2^20 real clock pulses. If my maths are correct therefore a change of +/-1 should equate to about 0.0824 seconds per day.

/* RTC init function */
static void myMX_RTC_Init(void)
{
int up=RTC_SMOOTHCALIB_PLUSPULSES_RESET;
int calibrate= -Option.RTC_Calibrate;
  /* USER CODE BEGIN RTC_Init 0 */
 
  /* USER CODE END RTC_Init 0 */
 
  RTC_TimeTypeDef sTime;
  RTC_DateTypeDef sDate;
 
  /* USER CODE BEGIN RTC_Init 1 */
 
  /* USER CODE END RTC_Init 1 */
 
    /**Initialize RTC Only
    */
  hrtc.Instance = RTC;
  hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
  hrtc.Init.AsynchPrediv = 7;
  hrtc.Init.SynchPrediv = 4095;
  hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
  hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
  hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
  hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
  if (HAL_RTC_Init(&hrtc) != HAL_OK)
  {
    _Error_Handler(__FILE__, __LINE__);
  }
  if (HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN) != HAL_OK)
  {
  _Error_Handler(__FILE__, __LINE__);
  }
 
  if (HAL_RTC_GetDate(&hrtc, &sDate, RTC_FORMAT_BIN) != HAL_OK)
  {
  _Error_Handler(__FILE__, __LINE__);
  }
  RtcGetTime();
  if(sDate.Year<18){
 
    /**Initialize RTC and set the Time and Date
    */
	  sTime.Hours = 0x0;
	  sTime.Minutes = 0x0;
	  sTime.Seconds = 0x0;
	  sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
	  sTime.StoreOperation = RTC_STOREOPERATION_RESET;
	  if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
	  {
		  _Error_Handler(__FILE__, __LINE__);
	  }
 
	  sDate.WeekDay = RTC_WEEKDAY_MONDAY;
	  sDate.Month = RTC_MONTH_JANUARY;
	  sDate.Date = 0x1;
	  sDate.Year = 0x0;
 
	  if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
	  {
		  _Error_Handler(__FILE__, __LINE__);
	  }
  }
  if(Option.RTC_Calibrate>0){
	  up=RTC_SMOOTHCALIB_PLUSPULSES_SET;
	  calibrate=512-Option.RTC_Calibrate;
  }
  HAL_RTCEx_SetSmoothCalib(&hrtc, RTC_SMOOTHCALIB_PERIOD_32SEC, up, calibrate);
 
}

Thanks Clive.

I will have to download the examples, do I have to install the latest cubemx , which wil instalkl the examples?

Scott

Thanks Peter

I will look into this. I am only using the 32.768KHz as the external crystal, what does it calibrate it against? Wouldnt it need a known frequency to calibrate against?

Scott

Peter Mather
Associate III

"Wouldnt it need a known frequency to calibrate against?"

The real world :)

"the clock is running about 5 second fast in 24 hours"

You would start with a value of -5/0.0824  = -61

this converts to

HAL_RTCEx_SetSmoothCalib(&hrtc, RTC_SMOOTHCALIB_PERIOD_32SEC, RTC_SMOOTHCALIB_PLUSPULSES_RESET, 61);

I you were 5 seconds slow it would be

HAL_RTCEx_SetSmoothCalib(&hrtc, RTC_SMOOTHCALIB_PERIOD_32SEC, RTC_SMOOTHCALIB_PLUSPULSES_SET, 512-61);

Typically an HSE supplied source, or you measuring it via MCO pin output on a test fixture.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

They should be in the repository if you have previously installed the L4 libraries. You can alternately pull the CubeL4 ZIP file an unpack and use that.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..