2013-09-06 5:32 AM
I'm trying to calibrate the difference of 512Hz at the out where PC13 possess 511.936Hz which causes about 10 seconds per day delay in the RTC. I'm making the form below, I wonder where I'm going wrong, not because it was effective, I do not find application notes with the correct sequence programming
// ((511.936-511.968)/511.9868) x 1 E06 = -62,5// Looking in calibration table, the nearest compensation value is 65// And then: status_error = RTC_CoarseCalibConfig(RTC_CalibSign_Positive, 65);status_error = RTC_CoarseCalibCmd(ENABLE); Does not effect !!!!!!! Somebody help me #calibration-rtc-stm32-f205We’re moving the ST Community to a new platform to give you a better and more reliable community experience.