2017-08-16 9:45 AM
I have a problem with STM32F415RG....
My project has two system of wakeup from standby, first is PA0 pin and other RTC Alarm.
If i put a single way of wakeup, like only PA0 wakeup work, if i put only RTC ALARM wakeup work, when i put both, not work...
I make many test:
When i put a alarm 30 seconds after standby, and i move the PA0 pin before the ALARM start, wakeup from pin work
When i put a alarm 30 seconds after standby and i wait the RTC ALARM, the system not start and not start anymore also from PA0 pin
Someone has same problem ?
Sorry for my english
2017-08-16 1:17 PM
Dear marco,
See our Errata 2.1.5 and apply the workaround.
http://www.st.com/resource/en/errata_sheet/dm00037591.pdf
Cheers,
STOne -32
2017-08-16 2:01 PM
I have already used the workaround but not work, anyway the result is the same.
Can you show me a little working example with ALARM A + PA0 Wake up with External Crystal 32768 ?
2017-08-17 11:05 AM
I found the problem....when enter on standby, i have PA0 pin high.....
2017-08-17 11:54 AM
Hi Marco,
Nice to see you solved it. Good job.
Cheers,
STOne-32.
2017-08-19 10:06 AM
But i suggest to correct the datasheet, because inside the only note is:
'Note: An additional wakeup event is detected if the WKUP pin is enabled (by setting the EWUP bit) when the WKUP pin level is already high.'
But you don't say that RTC Alarm not work if pa0 pin is high during WKUP pin enabling.
So if you enable RTC ALARM, push high pa0_pin and enable it throught EWUP, RTC ALARM will not work.
Please check it
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.