cancel
Showing results for 
Search instead for 
Did you mean: 

RM0433, 59.5.8 Microcontroller debug unit (DBGMCU): Typo or hidden feature?

Uwe Bonnes
Chief
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee

Hi @Uwe Bonnes​ ,

Please note that typo is fixed in the revision 6 of RM0433.

And now I think the secret is revealed with the announcement of STM32H7 dual-core described in RM0399.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Uwe Bonnes
Chief

Ops: I missed the content.

RM0433, 59.5.8 Microcontroller debug unit (DBGMCU) writes on page 3131:

"They are also accessible by both processor cores at base address 0x5C001000"

Probably "by both the processor and the debugger is meant"

Please clarify

Amel NASRI
ST Employee

Hi @Uwe Bonnes​ ,

Welcome to our Community Platform!

It is a typo. Thanks for highlighting.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Amel NASRI
ST Employee

Hi @Uwe Bonnes​ ,

Please note that typo is fixed in the revision 6 of RM0433.

And now I think the secret is revealed with the announcement of STM32H7 dual-core described in RM0399.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.