2016-07-04 10:33 AM
Hi
could anyone give a difference between reset the stm32f4 and power on/off stm32f4?2016-07-04 01:07 PM
SRAM Content?
2016-07-04 03:43 PM
2016-07-04 04:03 PM
I'm still a little cloudy on what the question is...
External devices lacking an asynchronous reset, and not connected to the STM32's NRST, clearly *aren't* going to reset when the device does.2016-07-05 06:08 AM
i will look at it clive ...thank you
2016-07-05 06:19 AM
I am not familiar with this IMU, it's connectivity to your system, or the software that runs in it.
Suggest you review the code in the IMU, and do some debugging/diagnostics there.2016-07-05 10:00 AM
Can we try not destroying the thread integrity.. it is something I find highly annoying.
From:emb_begin
Posted:Tuesday, July 05, 2016 12:43 AM
Subject:Reset and power
its for IMU(
inertial measurement unit
). could you also tell for sram also?From: emb_begin
Posted: Tuesday, July 05, 2016 3:08 PMSubject: Reset and powerlet me tell you what i does...
STM controller is connected to the IMu... i always flash the program using eclipse to stm controller and then press the reset button then the program execute and i can see the output on usárt...For IMU, i have to flash the code and then do the power off/on instead of press the reset..i dont know why its like that ...kindly explain clive