2023-04-04 4:57 AM
We are looking for a replacement of NXP microcontroller LPC1764FBD100. Can you please suggest a suitable ST Microcontroller?
Solved! Go to Solution.
2023-04-04 5:45 AM
Depending on your specific requirements, there are many STM32 that could be used instead of the LPC1764FBD100. However, it should be noted that no pin-compatible is possible, so a new circuit and a rewrite of the programme are necessary.
You can, however, look at, for example:
Hope that helps?
Regards
/Peter
2023-04-04 5:36 AM
Hello @Chaitanya ,
It offers products combining very high performance, real-time capabilities, digital signal processing, low-power / low-voltage operation, and connectivity, while maintaining full integration and ease of development.It offers products combining very high performance, real-time capabilities, digital signal processing, low-power / low-voltage operation, and connectivity, while maintaining full integration and ease of development.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-04 5:42 AM
Hi @KHALSI_Foued ,
I guess, you have missed to suggest the alternate part.
2023-04-04 5:45 AM
Depending on your specific requirements, there are many STM32 that could be used instead of the LPC1764FBD100. However, it should be noted that no pin-compatible is possible, so a new circuit and a rewrite of the programme are necessary.
You can, however, look at, for example:
Hope that helps?
Regards
/Peter
2023-04-04 5:49 AM
Thanks @Peter BENSCH . I will check the suggested parts.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.