Remapping of TIM1 pins PROBLEM
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2009-07-09 2:02 AM
Posted on July 09, 2009 at 11:02
Remapping of TIM1 pins PROBLEM
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 3:29 AM
Posted on May 17, 2011 at 12:29
Hey
I've got an STM32F103VBH6 processor. Now I'd like to remap the TIM1 pins from ''no remap'' to ''full remap'' and generate a PWM on these pins. I tried it by using the command: GPIO_PinRemapConfig(GPIO_FullRemap_TIM1, ENABLE); Without this command I get the PWM signal on the pins of the ''no remap'' configuration. Using this command generates no signal on no pin. ------ Here is my program for the REMAPPED pins (which doesn't work): ------ GPIO_StructInit(&GPIO_InitStructure); /* TIM1 and GPIOE clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1 | RCC_APB2Periph_GPIOE, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9| GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOE, &GPIO_InitStructure); GPIO_PinLockConfig(GPIOE, GPIO_Pin_9 | GPIO_Pin_11 | GPIO_Pin_13); /* Remaping of the TIM1 pins */ GPIO_PinRemapConfig(GPIO_FullRemap_TIM1, ENABLE); ------ This is the program of the NOT REMAPPED pins (which works fine): ------ GPIO_InitTypeDef GPIO_InitStructure; /* TIM1, GPIOA and GPIOB clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1 | RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB, ENABLE); /* GPIOA Configuration: Channel 1, 2, 3 and 4 Output */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9| GPIO_Pin_10 | g GPIO_Pin_11; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); /* GPIOB Configuration: Channel 1N, 2N and 3N Output */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_Init(GPIOB, &GPIO_InitStructure); Is there anything I've forgotten? Thanks for help. [ This message was edited by: davidhauser on 10-04-2008 17:56 ]Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 3:29 AM
Posted on May 17, 2011 at 12:29
for remapping you have to enable the AFIO clock if in case you have't done it.
/* AFIO clocks */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 3:29 AM
Posted on May 17, 2011 at 12:29
i am trying to use TIM3 Channel 1 as PWM from PC6 as AF; but the brigthness doesnt change. what am i doing wrong?? pls help...
here is the code: RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM3 , ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); GPIO_InitTypeDef GPIO_InitStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; //this pin functions as AF; when remapping GPIO_PinRemapConfig(GPIO_FullRemap_TIM3, ENABLE); /*GPIOC Configuration: TIM3 channel 1 */ /* make sure that C port is opened in RCC*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC, &GPIO_InitStructure); TIM_Cmd(TIM3, DISABLE); TIM_ARRPreloadConfig(TIM3, ENABLE); /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 999; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); /* PWM1 Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_Channel = TIM_Channel_1; TIM_OCInitStructure.TIM_Pulse = 500; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OCInit(TIM3, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Enable); TIM_ARRPreloadConfig(TIM3, ENABLE); /* TIM3 enable counter */ TIM_Cmd(TIM3, ENABLE); TIM_SetCompare1(TIM3,0x10);