cancel
Showing results for 
Search instead for 
Did you mean: 

Regarding the USB Support Libraries in Eclipse with Arm Development board

naman
Associate II
Posted on February 11, 2015 at 16:37

Hi,

I bought a Decawave EVK1000 Kit (http://www.decawave.com/products/evk1000-evaluation-kit) which uses ST libraries to provide USB Support and enable USB TO SPI functionality on the kit. I have the source code for the application which runs on the EVK1000 Kit but I do not have the ST libraries to support USB TO SPI functionality because of which the USB Support is not enabled and I am not able to use USB TO SPI function of the kit. I contacted the Decawave team and they sent me this link: http://www.st.com/web/en/catalog/tools/PF257882 which I think is the latest but even after integrating the libraries with the source code of EVK1000 Kit it gives errors like ''Fatal error: usb_conf.h missing : No File or directory''. When I look in to the libraries folder, it still has some missing files. I want to integrate the ST USB Support libraries with the source code of EVK1000 Kit to enable the USB Support on the kit and use its USB TO SPI functionality. I hope I have made myself clear. I know this might be a long shot but if anyone has any idea about such issue or has worked with EVK1000 board, please let me know.

Thanks a lot.

Naman Kumar

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0