Skip to main content
SN.1
Associate
July 14, 2020
Question

Regarding STM32L4R9A1 Evaluation Kit Octa Flash Reading Device ID

  • July 14, 2020
  • 0 replies
  • 919 views

Hi,

I have purchases STM32L4R9AI Discovery Kit, It has Macronix Octa Flash (MX25LM51245G).

I am trying to read the device ID In OCTA SPI Mode but unable to achieve the same.

Does any one has the code or the LAB Tutorial on the same.

I have gone through AN5050 App note on Octa flash interface.

Please help me with the inputs.

I have attached the project below.

BR

SN1

This topic has been closed for replies.