cancel
Showing results for 
Search instead for 
Did you mean: 

Real-time command execution STM32F407

sergej
Associate II
Posted on July 01, 2012 at 13:57

Hi, everyone.

Testing STM32F407.

Runs it at 168 MHz (5.92 ns cycle), FLASH-> ACR = FLASH_ACR_DCEN | FLASH_ACR_ICEN | FLASH_ACR_PRFTEN | FLASH_ACR_LATENCY_5WS.

Outstanding at the PA1 a simple square wave:

  PM_(RCC->AHB1ENR, RCC_AHB1ENR_GPIOAEN) = 1;                           // GPIOA clock enabled

  PM_(GPIOA->MODER, GPIO_MODER_MODER1_0) = 1;                           // PA1 - General purpose output mode

  GPIOA->OSPEEDR |= GPIO_OSPEEDER_OSPEEDR1;                             // PA1 - 100 MHz High speed

while (1)

{

GPIOA-> BSRR = GPIO_BSRR_BS_1;

GPIOA-> BSRR = GPIO_BSRR_BR_1;

GPIOA-> BSRR = GPIO_BSRR_BS_1;

GPIOA-> BSRR = GPIO_BSRR_BR_1;

GPIOA-> BSRR = GPIO_BSRR_BS_1;

GPIOA-> BSRR = GPIO_BSRR_BR_1;

GPIOA-> BSRR = GPIO_BSRR_BS_1;

GPIOA-> BSRR = GPIO_BSRR_BR_1;

GPIOA-> BSRR = GPIO_BSRR_BS_1;

GPIOA-> BSRR = GPIO_BSRR_BR_1;

}

Compiled as follows:

STR r1, [r0, ♯ 0x18]

STR r2, [r0, ♯ 0x18]

STR r1, [r0, ♯ 0x18]

STR r2, [r0, ♯ 0x18]

STR r1, [r0, ♯ 0x18]

STR r2, [r0, ♯ 0x18]

STR r1, [r0, ♯ 0x18]

STR r2, [r0, ♯ 0x18]

STR r1, [r0, ♯ 0x18]

STR r2, [r0, ♯ 0x18]

B | L1.6 |

On the oscilloscope can see this signal (Attachments img)

https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Attachments/23318/01.png

This means that the Branch instruction is actually executed in 3 cycles?

I have to debug in Keil stm32f4discovery.

At the Branch instruction cycle counter in the Keil (States) increased by 1.

In addition, using SysTick and DWT-> CYCCNT, they are also incremented by 1 for instructions Branch.

Why is it so?

#art-gpio-ahb
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on July 01, 2012 at 15:21

Why is it so?

 

Perhaps the pipeline stall is charged to the first store, along with whatever cache/prefetch introduces.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jpeacock2399
Associate II
Posted on July 01, 2012 at 23:12

First check the STM32F407 errata.  There's a warning that not all 'F407 parts (especially those on STM3240G boards, mine has no ART) have the ART flash accelerator.  Make sure your unit has the right product ID.  Without the ART instruction time (assuming no stall writing to AHB) instructions in flash will have a minimum of 5 wait states.

Second, the GPIOs run asynchronous to internal flash.  All you are testing for is the bus stall on writing to the AHB bus, not the flash speed.  A better test might be to execute a few tens of  instructions (no I/O) toggle the GPIO, the run the same code sequence again to generate your ssquare wave.  Look at the GPIO specs, all it can do is toggle at 100MHz, slower than flash.  Your program stalls waiting for the GPIO to cathc up.
spinazze
Associate
Posted on July 02, 2012 at 10:48

Hi Jack,

sorry but as I read from your message, all the 'F407 with silicon revision A don't have ART Accelerator???

All the 'F407 that I have are revision A, do you know when revision Z will be available?

Best Regards,

Alberto

Posted on July 02, 2012 at 22:33

There is an issue with the prefetch queue at lower voltages on the F2's, but the cache allegedly works. On the F4 A's the prefetch queue doesn't work. Presumably a critical path in there somewhere that didn't find closure.

https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Attachments/22412/2012_STM32%20Technical%20Updates%20-%20Issue%pdf

For availability call your local ST rep or FAE, there is very low participation here.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
sergej
Associate II
Posted on July 04, 2012 at 20:34

> Clive1, Sunday, July 01, 2012 3:21 PM

> Perhaps the pipeline stall is charged to the first store, along with whatever cache / prefetch introduces.

Thank you.

I use Z revision.

I read STM PM0081 Flash memory interface (ART - all for one cycle).

I read ARM Processor instruction timings (If branch taken, pipeline reloads (two cycles are added)).

I can not understand the branch should be executed in one cycle or up to 3 cycles?

> Jack Peacock, Sunday, July 01, 2012 11:12 PM

> First check the STM32F407 errata.

Thank you. I read STM32F407 errata.

> Second, the GPIOs run asynchronous to internal flash.

In my opinion it does not matter.

GPIO can have a slight delay.

But all the instructions should be followed consistently.

> A better test might be to execute a few tens of instructions (no I / O) toggle the GPIO

I added a 100 x nop

I use GPIO to control the run-time.

All debugging tools show a cycle for the branch, but actually three cycles.

> Look at the GPIO specs, all it can do is toggle at 100MHz

100 MHz are the two switch 1 -> 0 -> 1, ie 168/2 = 84 MHz max.